FB#.RESKTR

Description

This parameter sets the resolver nominal transformation ratio. It affects the resolver excitation output amplitude.

The value is obtained from the resolver data sheet.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0.001 to 50.000

Default Value

0.5

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

FB1.RESKTR

3500h

04h

Unsigned16

-

1000:1

Read/Write

No

FB2.RESKTR

3501h

04h

Unsigned16

-

1000:1

Read/Write

No

FB3.RESKTR

3502h

04h

Unsigned16

-

1000:1

Read/Write

No

FB4.RESKTR

3503h

04h

Unsigned16

-

1000:1

Read/Write

No

FB5.RESKTR

3504h

04h

Unsigned16

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

30140

1

30140 (0x75bc)

FB1.RESKTR

Unsigned16

Read/Write

Yes

30141

1

30141 (0x75bd)

FB2.RESKTR

Unsigned16

Read/Write

Yes

30142

1

30142 (0x75be)

FB3.RESKTR

Unsigned16

Read/Write

Yes

30143

1

30143 (0x75bf)

FB4.RESKTR

Unsigned16

Read/Write

Yes

30144

1

30144 (0x75c0)

FB5.RESKTR

Unsigned16

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.RESKTR

30140

Float

Read/Write

-

FB2.RESKTR

30141

Float

Read/Write

-

FB3.RESKTR

30142

Float

Read/Write

-

FB4.RESKTR

30143

Float

Read/Write

-

FB5.RESKTR

30144

Float

Read/Write

-